- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Maximum frequency
Function
Set the maximum value of the frequency output from the inverter. This frequency is also the criteria of acceleration and deceleration time.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.