- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
E-29: Control power option failure
Cause:
E-29 Control power option failure is caused by a failure of externally supplied control power into the +SU and CC terminals on the ASD. Typically this can mean one of the following.
1) Failure of the external control power supply (<20VDC).
2) The setting of Parameter F647: Control power option failure detection is incorrect.
Clearing:
Clearing this fault requires restoration of the control power to the drive
1) Verify that the external control power supply is providing a minimum of 20VDC on the input terminals +SU and CC. If not, service or replace the power supply.
2) If external control power is not being used, set [F647] = “0”.
Inspect the motor and driven equipment for issues prior to clearing any faults.
Use one of the following methods to clear the fault.
? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips
Discussion
E-29 indicates that externally supplied 24VDC power for control has been lost for any of a variety of reasons.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.