- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
E-26: CPU2 fault
Cause:
E-26 is caused by a failure of CPU2 in the drive.
Clearing :
Cycle power on the unit, if the fault re-occurs the drive CPU2 is most likely damaged and the unit will need to be serviced or replaced. Discussion
E-26 fault is fairly rare and almost always indicates that the drive has incurred some damage to CPU2. If the fault can be cleared then normal operation can be resumed but it is best to monitor the unit for future trips.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.