E-11: Brake answer error

Cause:
The E11 Brake Answer error fault occurs when the system does not reply within the time specified by parameter F63): brake answer wait time

Clearing:

Verify that the brake answer signal is correctly connected and is activating properly.

Check the setting of F630 is longer than the time it takes for the brake answer signal to activate.

Inspect the motor and driven equipment for issues prior to clearing any faults.

Use one of the following methods to clear the fault.

? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips

Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top