AS3 Troubleshooting
Automatic Acc/Dec
This is a parameter that automatically adjusts the acceleration/deceleration time according to the load condition to prevent an overcurrent trip during acceleration/deceleration.
Selecting a setting value
1: Automatic Acc/Dec
The acceleration/deceleration time is adjusted automatically in the range in which the output current does not exceed the rated current of the inverter. The adjustment range is 1/8 to 8 times as long as the time set with [ACC: Acceleration time 1] and [dEC: Deceleration time 1]. If you set suitable values for the average load with [ACC: Acceleration 1] and [dEC: Deceleration 1] in advance, it will be easy to deal with load fluctuation.
2: Automatic Acc only
Only the acceleration time is adjusted automatically. The speed is decelerated according to the setting of [dEC: Deceleration time 1].
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.