AS3 Troubleshooting
Terminal FP function 1
Output terminal parameter setting
Acc/Dec completed signal is the default setting for output terminal [FP].
When you want to output the inversion signal (OFF signal), set “7”.
? The signals can be also output from the other output terminals depending on the parameter setting.
When you want to output the signals from the [FLA]-[FLB]-[FLC] relay logic output terminals, set at [F132: Terminal FL function]. When you want to output the signals from the terminals [R1A]-[R1C], set at [F133: Terminal R1 function 1]. When you want to output the signals from the terminals [R2A]-[R2C]. set at [F134: Terminal R2 function ].
? When the run command (Fwd signal or Rev signal) is OFF, the Acc/Dec completed signal is also OFF.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.