- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
E-22: Embedded Ethernet fault
Cause:
E-22 is caused by a failure of internal Ethernet communications in the drive.
Clearing :
Inspect the motor and driven equipment for issues prior to clearing any faults.
Use one of the following methods to clear the fault.
? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips
Discussion
E-22 fault occurs when a problem arises in the ASD onboard Ethernet communication module. If the fault can be cleared using one of the methods above, normal operations can be resumed but the drive should be monitored for proper operation.
If the fault cannot be cleared, the unit will need to be serviced or replaced.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.