24 Apr 2025

Toshiba International Corporation Unveils RemotEye® 5 IIoT Network Card: Revolutionizing UPS Management with Predictive Capabilities

HOUSTON, TX—April 24, 2025—Toshiba International Corporation (TIC) proudly announces the launch of the RemotEye® 5 IIoT (Industrial Internet of Things) network card, the latest advancement in Uninterruptible Power System (UPS) monitoring management solutions. This next-generation UPS monitoring device introduces groundbreaking features designed to enhance monitoring with predictive capabilities, further solidifying Toshiba’s reputation for excellence in UPS management and monitoring.

“RemotEye® 5 transcends traditional monitoring by incorporating state-of-the-art predictive capabilities powered by machine learning, crucial for maintaining uninterrupted power systems,” stated Greg Mack, Senior Vice President and General Manager of the Toshiba Power Electronics Division. “This new generation of RemotEye® 5 equips users with real-time, remote access to informed decision-making for their UPS installations.”

Renowned for its reliable and user-friendly UPS monitoring, RemotEye® 5 offers comprehensive real-time control, predictive monitoring, and detailed analysis of UPS operations. The intuitive built-in software can automatically initiate an orderly shutdown of connected servers, minimizing data loss risk. Notably, RemotEye® 5 introduces one of the industry’s first UPS load forecasting features, utilizing machine learning to support capacity planning for critical applications.

This release marks the debut of an advanced machine learning model for load forecasting within the RemotEye® 5 system. By continuously monitoring load and analyzing trends on-site, data security is maintained without leaving the network. This load forecasting capability is instrumental in optimizing load management and enabling proactive load transfer between UPSs, essential in an AI-driven landscape with its increasing power demands.

Universal communication protocols compatible with RemotEye® 5 include Modbus TCP & RTU, BACnet IP, HTTP/HTTPS, and SNMP, alongside compatibility with IPv6. Enhanced hardware features include a 1 Gbps Ethernet interface, significantly improving data deliverability and reducing latency for real-time applications.

Complementing the RemotEye® 5, Toshiba also offers an updated Environmental Monitoring Device (EMD), providing real-time temperature and humidity updates. Users can daisy-chain up to eight EMDs into one RemotEye® 5 unit, offering enhanced insights into the UPS environment.

About Toshiba International Corporation

Toshiba International Corporation (TIC) is a Toshiba America Inc. (TAI) Group Company, a wholly owned subsidiary of Toshiba Corporation, and comprised of four divisions – Motors & Drives, Automotive, Power Electronics and Transmission & Distribution. Headquartered in Houston, Texas, TIC provides application solutions to a wide range of industries including general industrial, oil and gas, utilities, datacenters, renewables, HVAC, water/wastewater, and mining. For more information about TIC, please visit www.toshiba.com/tic.

About the TIC Power Electronics Division

The TIC Power Electronics division has more than 38 years of experience in uninterruptible power systems in North America. Toshiba produces a versatile range of single-phase and three-phase UPS solutions and accessories hallmarked for outstanding performance and reliability. Single-phase models range from 1 to 24 kW, while three-phase systems range from 10 to 2,000 kW, and three-phase parallel module systems range from 100 to 8,000 kW. These systems are suitable for a wide range of applications including data centers, telecommunication, retail, healthcare, broadcasting, and industrial.

For more information, please visit www.toshibaups.com

Scroll to Top