- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
E-43: Communication time-out (embedded Ethernet)
Cause:
E- 43 Communication time-ou t(embedded Ethernet) occurs when the embedded Ethernet module times out.
Clearing:
Check the Ethernet communication equipment and wiring.
Verify proper connection and that the PLC is communicating correctly to the onboard etherrnet.
Inspect the motor and driven equipment for issues prior to clearing any faults.
Use one of the following methods to clear the fault.
? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips
Discussion
This fault usually indicates either a wire break to the Ethernet communication module or a failure of the PLC or other device external to the ASD.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.