- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
E-39: PM control error
Cause:
E-39 PM control error occurs when a high motor current is detected either during auto-tuning or when the PM motor is starting.
Clearing:
Measure the motor inductance directly using an LCR meter and set this parameter directly.
Inspect the motor and driven equipment for issues prior to clearing any faults.
Use one of the following methods to clear the fault.
? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips
Discussion
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.