- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Guidance function
Parameters required for a special purpose can be displayed as a group and set collectively.
You can set necessary parameters easily by setting parameter groups in turn that are automatically formed for special purposes.
Purpose-specific guidance such as Embedded Ethernet setting, Preset speed operation, Motor 1,2 switching, and Motor parameter is provided.
How to use:
For example, set preset speed operation in the following procedure.
1 Select Guidance function “2: Preset speed operation” and press the [OK] key.
Parameters required for preset speed operation are displayed as a group.
Press the [OK] key with [CMOd: Run command select] on the top of the preset speed parameter group screen selected.
The selection screen of [CMOd] is displayed.
3 When you select [CMOd] and press the [OK] key, the screen returns to the preset speed parameter
group screen. Select the next parameter [FMOd: Frequency command select 1] and press the [OK] key.
By setting parameter groups similarly in turn, you can set necessary parameters easily.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.