Base frequency voltage 1

Function:
These parameters are used to set the rated voltage of the motor according to machinery. They are important parameters to decide the control range of the inverter.
Set the rated voltage (200 V, 220 V, etc.) of the motor according to the specifications of machinery. The inverter is controlled based on the rating of the motor specified with these parameters.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top