Frequency command select 1

Function

Select where to input a frequency command to the inverter
1: Terminal RR
Analog signal: Input a frequency command with 0 – 10 Vdc.
2: Terminal RX
Analog signal: Input a frequency command with -10 to +10Vdc.
3: Terminal II
Analog signal: Input a frequency command with 4 – 20 mAdc (0 – 20 mAdc).
4: Terminal AI4 (option)
The terminal [AI4] is included in the cassette option. Input a frequency command with an analog signal.
5: Terminal AI5 (option)
The terminal [AI5] is included in the cassette option. Input a frequency command with an analog signal.
10: Touch wheel 1 (power off or press OK to save)
Use the touch wheel on the operation panel to input a frequency command.
Even if you turn off the power supply without pressing the [OK] key, a frequency command value will be saved.
On the extension panel, use the up and down arrow keys to input a frequency command.
Even if you turn off the power supply without pressing the [ENT] key, a frequency command value will be saved.
11: Touch wheel 2 (press OK to save)
Use the touch wheel on the operation panel to input a frequency command.
Press the [OK] key, and a frequency command value will be saved.
On the extension panel, use the up and down arrow keys to input a frequency command.
Press the [ENT] key, a frequency command value will be saved.
12: Sr0
Set the value of the parameter [Sr0: Preset speed 0] as a setting value of a frequency command.
15: Terminal Up/Down frequency function
16: Pulse train
Input a frequency command with a pulse train signal (up to 30 kpps) to the terminals [S4] and [S5].
17: High resolution pulse train (option)
Input a frequency command with a high resolution pulse train signal to the input terminal.
20: Embedded Ethernet
Connect a communication cable to the Ethernet connector 1 or 2, and input a frequency command through the Ethernet communication.
21: RS485 communication (connector 1)
Remove the operation panel, connect a communication cable, and input a frequency command through the RS485 communication.
22: RS485 communication (connector 2)
Connect a communication cable to the RS485 communication connector 2 next to the control terminal block, and input a frequency command through the RS485 communication.
23: Communication option
Input a frequency command with a communication option command.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top