E-13: Abnormal speed error

Cause:

E-13: Abnormal speed error fault occurs when one or more of the following conditions occur:
1) When [Pt: V/f Pattern] = “0” to “9”, an over speed condition occurred.
2) When [Pt: V/f Pattern] = “10” to “11”, over speed occurred due to PG feedback failure
3) Due to overvoltage limit operation, the output frequency exceeded
[FH: Maximum frequency] +12 Hz
or
[FH] + [vL: Base frequency 1] x 0.1.

Clearing:

? Verify that input voltage is within specified range.
? If the application is producing a large amount of regenerative energy, install a dynamic braking resistor option.
? Check the wiring and programming of the PG encoder.

Inspect the motor and driven equipment for issues prior to clearing any faults.

Use one of the following methods to clear the fault.

? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips

Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top