- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting

Multi-rating select
Select an inverter/drive overload protection characteristic suited for the torque characteristic of the machinery.
Note) The setting value becomes 0 after execution, but a check mark is added to the previous setting value. An example of this is shown in the image above.
How to select a setting value
2: ND rating (120%-60s) (0 after execution)
Select this value when applying the machine with variable torque characteristic.
Example) Fan, pump, blower, etc.
3: HD rating (150%-60s) (0 after execution)
Select this value when applying the machine with constant torque characteristics.
Example) Conveyor, load transporting machinery, concrete mixer, compressor, making machine, machine tool, etc.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.