Is the AS3 available in 12-pulse or 18-pulse configurations? Sofia Osorio / April 21, 2026 The AS3 is not available in a 12-pulse configuration. 18-pulse input kits are available through Toshiba-approved panel shops.
Can I connect the keypad to a computer and load a configuration file? Sofia Osorio / April 21, 2026 Yes. Use PCM002Z software and a USB‑to‑mini‑USB cable. Configuration files can be transferred to the drive once main power is applied.