Can the keypad display output speed?
Yes. Parameter F702 can be used to apply a linear multiplier to display output speed.
Yes. Parameter F702 can be used to apply a linear multiplier to display output speed.
Yes.
Yes, but only for the primary function (Function 1).
QR codes can be generated for parameters, faults, or alarms by pressing the Info button (lowercase “i” icon). Scanning the QR code with a smartphone directs the user to the Toshiba website with relevant information and troubleshooting guidance for the specific fault.
Yes. The standard keypad supports Copy/Paste functionality between multiple AS3 drives. Parameters can also be transferred using Toshiba’s free ASD Pro Software.
Set parameter F750 to 2, then use the Hand/Auto button on the keypad to select the operating mode.