- QR Code Page
- Monitoring the Operation Status
Monitoring the Operation Status
Monitoring the Operation Status
Accessing Monitor Screen
from Keypad
Access the monitor screen from the default keypad
screen by pressing the F1 function key one time. If not on
the default keypad screen, please follow graphic below to
access the monitor screen.
screen by pressing the F1 function key one time. If not on
the default keypad screen, please follow graphic below to
access the monitor screen.
Monitor Mode Displayed Item Descriptions:
Descriptions
Input/output Terminals
Past trip 1 to 8
Communication status
Parts replacement alarm
Cumulative run time
Number of starting
Descriptions
Monitor Mode Displayed Item Descriptions:
- Direction of rotation Forward or Reverse inverter output direction.
Input/output Terminals
Displays the ON/OFF status of the following input/output terminals.
- Input terminal 1 (F, R, RES, S1...S4, S5)
- Input terminal 2 (DI11, DI12...DI16)
- Output terminal 1 (FP, FL,R1, R2)
- Output terminal 2 (DQ11, DQ12, R3, R4, R5)
- Output terminal 3 (R6, R7...R11)
Past trip 1 to 8
Past trip 1 to 8
- Past trip 1 is the record of the latest trip, Past trip 8 is the record of the oldest trip. If no trip information exists, โnErrโ is displayed.
Communication status
Communication status
- RS485 communication connector 1 and 2 status.
Parts replacement alarm
Parts replacement alarm
- Displays replacement alarms of the cooling fan, capacitor, etc.
Cumulative run time
Cumulative run time
- Inverter cumulative run time is display. The display unit is 100 hours and the minimum value 0.01 Is equal to 1 hour. To clear the value, set parameter [tyP: Default setting] to "5: Clear cumulative run time."
Number of starting
Number of starting
- The number of inverter starts is displayed. The display unit is one time and the maximum value is 9.99 million times. In the case of an LED display extension panel, the display unit is 10000 times and the minimum value 0.1 is equal to 1000 times. To clear the value, set [tyP: Default setting] to "12: Clear cumulative run time."
| Setting Value | Function Name | Display Unit | Settings for [F711: Monitor mode 1 display] to [F718: Monitor mode 8 display] |
|---|---|---|---|
| 0 | Output frequency | 0.1 Hz | |
| 1 | Frequency command value | 0.1 Hz | |
| 2 | Output current | 1%/[F701] setting | |
| 3 | Input voltage (DC detection | 1%/[F701] setting | |
| 4 | Output voltage | 1%/[F701] setting |