17Apr 2026

What is the temperature rating of the AS3?

Ambient operating temperature:

  • 14°F to 122°F (–10°C to +50°C) without derating
  • Up to 140°F (60°C) with derating

Stories Not Found

Stories Not Found

Scroll to Top