17Apr 2026

What is the overload rating of the AS3?

The AS3 offers dual overload ratings based on duty type:

  • Heavy Duty (HD)
    • 110% continuous
    • 150% for 60 seconds
    • 180% for 2 seconds on frames A1–A6
    • 165% for 2 seconds on frames A7–A8 (250–450 HP)
  • Normal Duty (ND)
    • 105% continuous
    • 120% for 60 seconds
    • 150% for 2 seconds

Stories Not Found

Stories Not Found

Scroll to Top