- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Region setting check
Function
When you select a region using in the setup menu at initial Power on, parameters such as the base
frequency of the motor is set automatically according to the selected region.
You can check the region that has been set or reset it by starting the setup menu.
Selecting a setting value
0: Setup menu starting
The setup menu to select the region where the inverter is used is started.
When you select the region, parameters such as the base frequency and the base frequency
voltage of the motor that are described on the separate table are automatically set.
? While the setup menu is started, you cannot return to the previous step even if you press the [ESC] key.
? Note that all parameters return to status of default setting and the trip history data is cleared.
1: Japan (read only)
2: Mainly North America (read only)
3: Mainly Asia (read only)
4: Mainly Europe (read only)
5: Mainly China (read only)
All of 1 to 5 are display to check the setting. Even if you select any of them and press the [OK] key, new setting cannot be made.
There is a mark at the right end of the region selected in the setup menu.
? The setting values of the parameters set with the setup menu can be changed as in the case of other parameters.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.