- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
EPHO: Output phase loss
Cause:
EPHO: Output phase loss typically occurs when one of the three output leads (U/T1, V/T2, W/T3) has become disconnected from either the drive or the motor.
Clearing:
Verify that all three output phases of the ASD are connected at both the drive and the motor terminals.
Inspect the motor and driven equipment for issues prior to clearing any faults.
Use one of the following methods to clear the fault.
? The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
? Activate a digital input that has been programmed to ?Reset? function
? Set the tyP (F007) Parameter to: 4: Clear past trips
Discussion
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.