- QR Code Page
- Simplified Operation
Simplified Operation
Parameter CMOd: Run command select
-
- 0: Terminal
Run/stop the inverter with an external ON/OFF signal.
-
- 1: Operation panel, Extension panel
Press the [RUN], [STOP] key on the operation panel to run/stop the inverter.
You can do it even on the optional extension panel.
-
- 2: Embedded Ethernet
Connect a communication cable to the Ethernet connector 1 or 2, and run/stop the inverter through the Ethernet communication.
-
- 3: RS485 communication (connector 1)
This has the operation panel mounted when shipped from the factory. Remove the operation panel and connect a communication cable, and you can run/stop the inverter through the RS485 communication.
-
- 4: RS485 communication (connector 2)
Connect a communication cable to the RS485 communication connector 2 next to the control terminal block. Then, you can run/stop the inverter through the RS485 communication.
-
- 5: Communication option
Run/stop the inverter with a communication option command.
Parameter FMOd: Frequency command select 1
- 1: Terminal RR
Analog signal: Input a frequency command with 0 – 10 Vdc.
- 2: Terminal RX
Analog signal: Input a frequency command with -10 to +10Vdc.
- 3: Terminal II
Analog signal: Input a frequency command with 4 – 20 mAdc (0 – 20 mAdc).
- 4: Terminal AI4 (option)
The terminal [AI4] is included in the cassette option. Input a frequency command with an analog signal.
- 5: Terminal AI5 (option)
The terminal [AI5] is included in the cassette option. Input a frequency command with an analog signal.
- 10: Touch wheel 1 (power off or press OK to save)
Use the touch wheel on the operation panel to input a frequency command.
Even if you turn off the power supply without pressing the [OK] key, a frequency command value will be saved.
On the extension panel, use the up and down arrow keys to input a frequency command.
Even if you turn off the power supply without pressing the [ENT] key, a frequency command value will be saved.
- 11: Touch wheel 2 (press OK to save)
Use the touch wheel on the operation panel to input a frequency command.
Press the [OK] key, and a frequency command value will be saved.
On the extension panel, use the up and down arrow keys to input a frequency command.
Press the [ENT] key, a frequency command value will be saved.
- 12: Sr0
Set the value of the parameter [Sr0: Preset speed 0] as a setting value of a frequency command.
- 15: Terminal Up/Down frequency
Input a frequency command with an Up/Down command to the input terminal.
- 16: Pulse train
Input a frequency command with a pulse train signal (up to 30 kpps) to the terminals [S4] and [S5].
- 17: High resolution pulse train (option)
Input a frequency command with a high resolution pulse train signal to the input terminal.
- 20: Embedded Ethernet
Connect a communication cable to the Ethernet connector 1 or 2, and input a frequency command through the Ethernet communication.
- 21: RS485 communication (connector 1)
Remove the operation panel, connect a communication cable, and input a frequency command through the RS485 communication.
- 22: RS485 communication (connector 2)
Connect a communication cable to the RS485 communication connector 2 next to the control terminal block, and input a frequency command through the RS485 communication.
- 23: Communication option
Input a frequency command with a communication option command.
Parameter tHrA: Motor overload protection current 1