OCL: Overcurrent (load side at startup)

Cause:
1) Short circuit occurred on the output side.
2) The motor and output side wiring have defective insulation.
3) Impedance on the motor is low.

Clearing:
1) Check the wiring on the output side.
2) Check the insulation on the output side.
3) Set [F613: Short circuit detection at start] to “2” or “3”.
(Note: To ensure the drive or machinery is running properly, separate the equipment and test, if necessary)

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top