- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Undercurrent detection level
Function:
When a current level set in [F611 : Undercurrent detection level] or less is detected for the period of time set in [F612: Undercurrent detection time] or more, the invertor trips and “UC” is displayed. After tripping (UC) alarm signal remains ON.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.