- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Power running torque limit level 1
Function
When the motor-generated torque reaches a certain level, the inverter reduce the torque by lowering the output frequency. You can select a constant output limit or a constant torque limit in the constant output zone.
Selecting a setting value
1) When torque limits are applied by the parameter setting values
Select from where to input a torque limit value at <F440: Power running torque limit input select 1> and <F442: Regenerative torque limit input select 1>.
As default setting, torque limits are applied by the parameter setting values.
Set the torque limit values for the power running and regenerative torques at <F441: Power running torque limit level 1> and <F443: Regenerative torque limit level 1>.
Set limit treatment of the constant output zone (weak magnetic field) at <F454: Torque limit in field weakening>. You can select either constant output limit <F454> = “0” (default setting) or constant torque limit <F454> =”1″.
2) When torque limits are applied by external signals
Torque limit value can be changed by external signals.
? When setting with input of 0 to 10 Vdc to terminal [RR]
Set “1” for <F440: Power running torque limit input select 1> and <F442: Regenerative torque limit input select 1>.
? When setting with input of -10 to 10 Vdc to terminal [RX]
Set “2” for <F440: Power running torque limit input select 1> and <F442: Regenerative torque limit input select 1>.
? When setting with input of 4 to 20 mAdc to terminal [II]
Set “3” for <F440: Power running torque limit input select 1> and <F442: Regenerative torque limit input select 1>.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.