Err6: Gate array faultCurrent detector fault

Cause:

Err6: Gate array fault occurs when there is a failure in the main gate array on the drives printed circuit board.

Clearing:

Cycle power on the unit. If the fault re-occurs, the unit will need to be serviced or replaced.
Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top