UtC3: Undertorque/Undercurrent

Cause:
Undertorque or undercurrent on the shock monitoring function was detected.

Clearing:
? Check the load.
? When no problem is found, check if the shock monitoring function setting is correct.
[F590: Shock monitoring] to [F598: Shock monitoring detection condition]
Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top