SOUT: PM step-out

Cause:
1) The load changed rapidly.
2) Sudden acceleration/deceleration occurs.
3) The motor shaft is locked up.
4) Output side phase has failed.

Clearing:
1) and 2) Increase the acceleration/deceleration time.
[ACC: Acceleration time1]
[dEC: Deceleration time 1]
etc.
3) Check the motor and release the lock.
4) Check the wiring on the output side.
Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top