- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
PrF: STO circuit fault
Cause:
1:Connection are not made correctly to device.
2: Different input level between [STOA] and [STOB].
3: Fault in Safe Torque off (STO) circuit.
Clearing:
Check safe torque off (STO) terminals are correctly connected on the control terminal strip.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.