- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Panel Fwd/Rev run select
Function
This parameter is used to select the direction of rotation of the motor during panel run.
The direction of rotation can be changed during run by using the [FWD/REV] key on the operation panel.
Selecting a setting value
0: Fwd run
When you press the [RUN] key on the operation panel, the motor runs forward.
Forward run/reverse run cannot be switched.
1: Rev run
When you press the [RUN] key on the operation panel, the motor runs reversely.
Forward run/reverse run cannot be switched.
2: Fwd run (switchable F/R by panel)
When you press the [RUN] key on the operation panel, the motor runs forward.
When you press the [FWD/REV] key during forward run, the motor starts running reversely. When you press the [FWD/REV] key again, the motor starts running forward.
The command given before “MOFF” display is remained at the power off.
3: Rev run (switchable F/R by panel)
When you press the [RUN] key on the operation panel, the motor runs reversely.
When you press the [FWD/REV] key during reverse run, the motor starts running forward. When you press the [FWD/REV] key again, the motor starts running reversely.
The command given before “MOFF” display is remained at the power off.
Direction of rotation of motor
You can check the direction of rotation of the motor on the display.
? This function is valid when the motor is run/stopped from the operation panel or extension panel ([CMOd: Run command select] = “1”).
? In the case of terminal run, setting with [Fr: Panel Fwd/Rev run select] is invalid.
Switch forward/reverse run with the terminal [F] and the terminal [R].
Terminal [F]: Fwd run
Terminal [R]: Rev run
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.