- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Motor pole number for communication
Sets the motor poles used internally by the drive for speed calculations when speed is being set via communication.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.