Status area display of operation panel

Determines which monitor value appears in the status area display on the main operation screen
This is the value to the left of the RUN/STOP indication on the very top line of the main display.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top