- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Pulse output step of input cumulative power
Function
Every time the integral input power reaches the cumulative power unit set by [F667: Pulse output step of input cumulative power], pulse signal can be output. You can display the power by pulse count without an external power meter.
Pulse output width is set by [F668: Pulse output width of input cumulative power].
Setting the parameters
This is a setting for pulse output from terminal [FP].
Set [F130: Terminal FP function 1] = “180: For input cumulative power”
Set the integral power unit with [F667: Pulse output step of input cumulative power], and set the pulse output width with [F668: Pulse output step of input cumulative power].
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.