Panel jog run

Function
Jog run represents inching the motor.

When you input a jog run signal, the inverter immediately outputs a jog run frequency regardless of the set acceleration time.

You can start/stop jog run even on the operation panel.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Scroll to Top