- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Pulse train input point 2 input value
Function
These parameters set the frequency command characteristics by pulse train input.
You can use the terminals [S4] and [S5].
When you want to use pulse train input, set [FMOd: Frequency command select 1] (or [F207: Frequency command select 2]) to “16: Pulse train”.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.