- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
Err3: ROM fault
Cause:
ERR3: ROM fault typically occurs due to a fault or failure on the ASD internal ROM memory.
Clearing:
Cycle power on the unit. If the fault re-occurs, the unit will need to be serviced or replaced.
Discussion
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.