FAQs

What type of energy savings can be achieved with an adjustable speed drive?

Using an adjustable speed drive (ASD) on an AC motor can provide significant energy savings depending on the application. By varying motor speed to meet actual process requirements, ASDs help minimize wasted energy, reduce inrush current, and maintain a near-unity power factor.

In variable torque applications, such as centrifugal fans and pumps, energy consumption decreases according to the affinity laws. For example, operating at 50% speed can require only about 13% of full-load power. In many installations, these efficiency improvements can lead to a relatively short return on investment.

 

Why use an adjustable speed drive?

An adjustable speed drive (ASD) regulates motor speed to match actual load requirements, which can lead to substantial energy savings, often up to 70% in variable torque applications such as fans and pumps.

Beyond energy efficiency, ASDs provide improved process control, motor overload protection, unlimited starting capability, and reduced mechanical and electrical stress. These benefits can help extend motor life and lower maintenance requirements in AC motor systems.

What is an adjustable speed drive?

An adjustable speed drive (ASD), also referred to as a variable speed drive (VSD) or variable frequency drive (VFD), is an electronic device that controls the speed and torque of an AC motor by varying the frequency and voltage of the electrical power supplied to it. This enables precise motor control, improved process performance, and potential energy savings in a wide range of industrial applications.

An ASD converts incoming AC power to DC through rectification, then inverts it back to a controlled three-phase AC output at variable frequency and voltage. This output allows the connected motor to operate at the desired speed. Adjustable speed drives are commonly applied in pumps, fans, compressors, conveyors, and other variable-torque systems.

Scroll to Top