Flagship EQP Global® Low Voltage Motor Series Now Available in IEC Compliant Motors
HOUSTON, TX — Aug. 6, 2018 — Toshiba International Corporation (TIC) today announced the cutting edge Efficiency, Quality, & Performance (EQP) Global low voltage motor series now includes IEC motors compliant with the requirements of IEC 60034. The
EQP Global IEC motor series
is designed for severe duty applications, featuring IP55 ingress protection and a totally enclosed fan cooled (TEFC) enclosure.
“The new
EQP Global IEC motor series is our latest solution aimed at meeting the competitive demands of the global market,” said Mark Laber, Vice President and General Manager of the TIC Motors & Drives division.
The
EQP Global IEC motor series builds on 20 years of success with the EQPIII motor series, now with multiple design innovations resulting in one of the lowest cost-of-ownership products in the industry. The motor series is available in .75 to 45 kW with speeds ranging from 1,000 to 3,000 RPM. Additional features include:
- Dual-Frequency 50/60 Hz Design and Listed on Nameplate
- Dual-Voltage Frames 80-132; Single-Voltage Frames 160-225
- Multi-mount for 225 Frame (225M & 225S)
- Aluminum Frame with Removable Base for 90S through 160M Frames
- Cast Iron Frame 80M, 180 through 225 Frames
- Winding PTC Thermistors for > 160 Frame
About Toshiba International Corporation
Toshiba International Corporation (TIC) is a Toshiba America Inc. (TAI) Group Company, a wholly owned subsidiary of Toshiba Corporation, and comprised of four divisions - Motors & Drives, Automotive, Power Electronics and Transmission & Distribution. Headquartered in Houston, Texas, TIC provides application solutions to a wide range of industries including general industrial, oil and gas, utilities, datacenters, renewables, HVAC, water/wastewater, and mining. For more information about TIC, please visit
www.toshiba.com/tic.
About the TIC Motors & Drives Division
The TIC Motors & Drives division, which offers a full range of low and medium voltage motors, adjustable speed drives, motor controls, and power apparatus & components, is anchored by a totally integrated manufacturing process; research and development, design, engineering, production and manufacturing, and aftermarket service and support are all commandeered under one roof. With the capability to test products together as a system before sending out into the field, TIC ensures the highest level of quality, performance, and reliability.